Other Parts Discussed in Thread: TLV431, UCC25630-1EVM-291, TL431
Hi,
we are building an LLC power stage with the following specs
VIN,NOM = 310VDC, VOUT = 85VDC, POUT = 600W
Simplified schematic attached for more details
After some initial fixes, we are now experiencing the following issues:
- Controller is switching but output voltage is not regulated.
Switching frequency keeps reducing (and output voltage increasing, as expected) even well after target voltage is reached - Without the Zener circuit to prevent optocoupler deep saturation, the controller does not start at all.
- Switching frequency changes with controller temperature (higher temp -> lower switching freq, and vice versa)
Here some scope acquisitions (@VIN = 280V POUT = 110W).
We thought of a problem on FB pin or mistakes on our voltage compensation loop.
Any suggestion or recommendation is welcome.
Many thanks.