Hi,
A problem occurs using TPS51200.
The input to the TPS51200 is as follows.
・ REFIN 0.75V
・ EN pin 3.3V
・ PGOOG pin 3.3V
・ VIN pin 3.3V
The desired output voltage is 0.75V. After mounting on PCB, 0.75V is output normally. However, the output voltage changes to 1.0V at a certain timing. If you have any advice on the cause of this phenomenon, please let me know.
Thanks,
Koki