Hi,
I have designed a DC-DC converter of +5.7V at 14A with 18-36V. It seems to be working good. I have followed the layout of Evaluation board of LM5117. The PCB is a 4-layer board and the copper weight on each layer is 2oz.
I see two problems when testing with a load of 6A.
1. There is a voltage drop of 0.25V as soon as I connect the load, but then voltage remains stable, 5.7V drops to 5.5V and this value remains the constant even after 15 minutes. Also, if I increase the load this drops also increases
2. PCB starts to get hot and after sometime it is quite hot and a bit difficult to touch.
I have attached the circuit for reference.
I look forward to hearing from you.
Many thanks
Kind Regards:
Mohsin