Hi,
My EV2400 programmer has stopped working suddenly. No LEDs on, the windows recognises that it is a TI device but neither the firmware updater neither the Battery Management Studio recognises it.
I checked the voltage on the I2C pull up lines and it shows 4.2V which might be some default value which means that its voltage rail is not programmed from the MCU..
What can I do?? Isn't possible to reprogram somehow the MCU? If electronically it is all good and might just need a reflashing of the memory.
I ordered the programmer from Ti store with the order number: T00548190, data placed: 10/02/2019.
Please advice!
Thanks,
Andras