Other Parts Discussed in Thread: BQSTUDIO
Hi, Ti suporters
Thanks for the help on previous threads.
now i am almost finishing my project but still have one more question before making the golden file.
when finishing the second learning cycle, the Qmax is learning well to the real capacity,
and I found that the Ra0 and Ra0x tables are both renewed as below.
There are diferent between on the last two values.
and Grid number already reach 15 and i performe the second learning cycle same as the first one
The Update Status is still stay in 0x06 after relaxing for more than 10hours.
1、if the Update Status is not change to 0x0E, does it mean the learning fialed?
2、if question 1 is true, what have i missed to fulfill to the 0x0E status.
3、or Can I make the golden file now.
The registers and bit register which are in relax stage for more than 10 hours are show as below.
Appreciate for all of your help, very much.