Hi team,
Could you please help confirm maximum start up time of TPS62065-Q1? In datasheet the typical value is 500us and no min and max value.
Thanks,
Scarlett
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could you please help confirm maximum start up time of TPS62065-Q1? In datasheet the typical value is 500us and no min and max value.
Thanks,
Scarlett
Hi Tanvee,
The EE is ADAS-AVM. Customer asks this out of OEM requirement to calculate max delay. I see from datasheet this spec is defined as active EN to 95% Vout. We only need to provide the tSTART value and customer will add the ramp time on their own. Can we provide the start-up time from IC perspective?
Thanks,
Scarlett
Hi Scarlett,
As I said earlier, it is not tested during device characterized that's the reason it is not simple to give accurate figure for maximum spec. According to device design, I would expect the start up time can vary up to ~10%. Customer can evaluate maximum spec accordingly.
Best regards,
Tanvee