This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: Can BQ25703A support LTO battery charger?

Part Number: BQ25703A

Hi team,

My customer is looking for LTO type battery charger and would like confirm if BQ25703A is able to support LTO type battery charger. thanks. 

Below is customer requirement and Battery spec.

Toshiba SCiBTm 2.9Ah cell

https://www.global.toshiba/ww/products-solutions/battery/scib/product/cell.html

model : MP146396PA

Nominal voltage :2.4V

Rated capacity :  2.9Ah

Input Voltage : 3.5V ~ 26V

Charging current : >2A

I2C host interface

can also support Solar input.

 

Thanks & Regards

Eddie Chou