I want a boost converter that takes 3.3V and converts to 300mA@3.6V. It needs to have a low quiescent current of less than 20uA, the load can go as low as 400uA. However when the load has a usb pluged into it the 3.6V output will rise to 5V. Will this feed back into the Vin input (3V3) if it is still enabled, and if so is their anything more appropriate