Other Parts Discussed in Thread: BQ79616
Hello,
in the datasheet of the BQ79616 a maximal balancing current of 240mA is stated. But this current appears also in the absolut maximum ratings. Furthermore, in the typical applications chapter the balancing resistor is specified to 10R. According to my calculation a resistor of 7.5R + Rdson would lead to a maximal current of 236mA. Is this still recommended, or is the recommendation based on the 10R resistor?
BR
Christian