This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62562: PMIC

Part Number: TPS62562

Hi Team,

I want to find a PMIC, it will be used in wearable. Blow are the requirements. Do you have any recommendation?

1.Vin is about 5V.

2.The number of output is about 5 to 6. The number of buck should be more than LDO.

3.Need two output can support less than or equal to 0.6V.

Best Regards,

Gust