Other Parts Discussed in Thread: LM25145
Hello, we are still working (with a lot of troubles...) on this design, . Now we are using this mos : SUD23N06.
With SUD23N06 we can get up to 13A withut problem. We need to set a current limit at 10A. Which is the correct way to do it?
The controller we are trying to realize has two identical power channel, I mean two LM5117 configured to source two indipendent 12v 10a channels.
The two channels are absolutely the same. They share the same schematic, but a different layout.
One channel now works, the other fails at power on. We can esclude schematic and/or pcb errors.
Could be design layout so critical?
Maybe our last chance will be switch from LM5117 to another device. Can you suggest a different power controller easier to configure and design with?
We need an output of 12V 10A from a 30-42Vdc input.
Thank you in advance
Francesco