Other Parts Discussed in Thread: BQ25730
Hello,
We are looking for a lithium ion battery charger IC that matches our requirement given below. Could you please help us in finding a suitable match for our requirement or suggest an alternate solution.
Battery Chemistry |
Lithium Ion |
No. of cells |
1S-4S or 1S-5S (Preferred) |
Charge Current |
Configurable between 100mA to 8A |
Current regulation accuracy |
+/- 1% or +/-10mA (whichever is greater) |
Max Battery pack voltage |
17.4V or 21.75V(Preferred) |
Voltage regulation accuracy |
+/-25mV |
Control Interface |
I2C, SMBus |
We have identified BQ25731 : What is the minimum charging current that can be set ? We 100mA. +/-10mA current. Kindly suggest IC which is close to this requirement.