Other Parts Discussed in Thread: LM3478, LM5155
I have used the LM5022 on a previous design, however with the friendly scalpers in HK purchasing all parts they can, it's in short supply like many other TI SMPS controllers and regulators. 59 weeks factory lead time for TPS54335ADDA? Ouch.
Looking at the selection I've found LM3478 as a potential replacement, it's not pin or function compatible but both can do the same job more or less. Is there a reason to prefer one over the other? LM5022 is somewhat more capable but nothing drastic as far as I can tell:
- Max Fsw is 1MHz vs 2.2MHz
- Operating voltage is 3-40V vs 6-60V
- Mad duty cycle is 100% vs 90%
- Error amplifier is transimpedance vs regular
- LM3478 does not support external sync, LM5022 does
None of these really matter for 12Vin 48Vout 0.5A boost converter I'm designing.
LM3478 has better supply situation although scalpers have been purchasing them like they were going out of fashion, with half a million or more in hoarded to China depending on variant. But you can still buy it in normal distributors, at least for now.