This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24314A: supported current exceeding 1.5A but below abs max ratings

Part Number: BQ24314A
Other Parts Discussed in Thread: BQ24381, BQ24382

Hi,

I'm currently looking into implementing battery protector IC BQ24314A onto my design. One of the issue I faced now is that the device is rated to support up to 1.5A and on my application when battery level is low my device may subject to current of up 1.8A when charging. Hence may I know if it's okay to continue to apply this device on my design? I did noticed that absolute max current rated at 2.0A hence had the intention to use this device. Thanks.

BR,

Leo