Hi Team,
Could you please help to simulate the rise time data at below condition? Thanks.
VIN = 3.3V
VBIAS = 3.3V
CT = 220pF
Cin = 1uF
CL = 1uF
RL = 10 ohm
Best regards,
Hardy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Hardy,
I will test this and get back to you by EOD 9/14; however, it should be fairly close to the table listed in the datasheet but with a small variation due to 3.3v on VBIAS.
Regards,
Kalin Burnside
Hi Kalin,
Thanks for your help.
Please let me know if you have any measurement data.
Best regards,
Hardy
Hello Hardy,
The table below includes the timing data from your conditions on the EVM on a lab bench:
Timing results (us) | ||||
Load | trise | ton | toff | tfall |
10 Ohm | 615.6 | 638.7 | 2.502 | 3.17 |
If you would like a simulation please let me know; however, the turn around time for simulations is typically 6 weeks.
Regards,
Kalin Burnside
Hi Kalin,
Thanks for your information.
If customer would like to let rise time < 500us, is using 0.1uF CL the easiest method?
Because using 5VBIAS that need to change layout. Or, do you have better suggestion?
Best regards,
Hardy
Hello Hardy,
You could place a low capacitance on the CT pin (floating 0 pF - 100 pF). That CL capacitor won't have a large effect on the rise time.
Regards,
Kalin Burnside