Hi,
I'm doing a simulation using PSpice for TI and TPS2116 model in Manual Mode but it seems not to work correctly. IN1 is fixed at 5V, IN2 at 3.3V, Mode is 0V (tied to GND), PR1 is 0V.In these conditions OUT is zero volt but standing from datasheet it should be at 5V. The model is not accurate in this working mode?
Unfortunately I have no TPS2116 samples on my hands to do a true test.
Thank you