This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65917-Q1: fail-safe inputs operated at >VRTC range

Expert 7280 points
Part Number: TPS65917-Q1

Dear team,

Just to double check: for the fail-safe inputs of TPS65917-Q1, it is pretty clear that no harm will be done the PMIC if these are driven up to 5V and the VRTC is only related to the logic levels of these pins, but I was wondering if there were any side effect on driving these pins at 3.3V or 5V ? Any extra leakage to expect ? anything else ?

Thanks a lot ! Slight smile

Best regards,

PA