How to use Pin Selected Rail states Config?
Refer below screeshot, I selected Pin Selected Rail States Config and set them. However, the Rail#5 is shut down when i configure rail#5 On/Off Operation only.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to use Pin Selected Rail states Config?
Refer below screeshot, I selected Pin Selected Rail States Config and set them. However, the Rail#5 is shut down when i configure rail#5 On/Off Operation only.
Thanks
Hi
For pin selected rail state(PSRS),
1. the on/off_config must be set to OPERATION
2. the GPI state decides whether the rail is on or off based on your settings.
I do not get what you mean rail 5 is off when configurating ON/OFF_COFIG to OPERATION? what's the setting before?
Please be noted, each time you change the ON/OFF_CONFIG, device is going to evaluate to decide whether the rail shall be on or off?
Regards
Yihe
Hi
The rail#5 is set None originally. I change rail #5 the on/off_config to Operation Only because i want to use PSRS to control all the rails using GPI1 and GPI2. However, the rail#5 shut down when i configure rail#5 On/Off Operation only. Does the rail enble have to be GPIs when use Operation only?
Thanks
Hi
Yes, please check this video.
PIN SELECTED RAIL STATE works only if the rail's on/off config is set to operation mode.
Regards
Yihe