Other Parts Discussed in Thread: TPSM84203,
Hello,
Context of my question : I’m developping a medical device. I will have a first AC/DC adaptator (external switching power supply) with an ouput of 24VDC as i need to power a stepper motor. I need also a DC/DC regulator to power a microcontroller and a remote control (with a small oled screen) (maximum 0.9 A globally, with almost always less than 300mA ) that has the 24VDC in input and outputs 3.3 V.
I want take care of the EMI specifications as i will have to pass some EMI tests (certainly CISPR11 class B). I don’t want to take any risk and i’m following the advice you wrote in the application note « Simplify low EMI design with power modules », that is, i’m trying to use one of your modules with integrated inductors. With the specifications i have (24V input, 3.3V output, 0.9A), i found two possibilities : LMZM23601v3 and TPSM84203.
In the datasheet of LMZM23601, the figure 8 shows the radiated EMI. It is under the level of the CISPR11 class B. It is not written clearly, but i suppose the measurements are with Quasi Peak, with 10 m of measuring distance, as the limit of CISPR11 class B drawn (30 dbuV/m and 37 dbuV/m) corresponds to these hypotheses. However, we can see on the curves that there is not a lot of margin as the radiated EMI measured is above 30 dbuV/m in the 300 MHz range and in the 500 MHz range.
If we look at the TPSM84203 datasheet, the figure 25 shows that the radiated emissions of the TPSM8403 is under a CISPR (which number ?) classe B at 10 meters (with the same values as before i.e. 30 dbuV/m and 37 dbuV/m). I suppose that the measurements are also with Quasi Peak, with 10 m of measuring distance. This time, for this module, the radiated emissions are much below (below 20 30 dbuV/m until 500 MHz).
The only difference for the boards used for the measurements is that the TPSM840203 EVM has more capacitors around the TPSM84203 (but no inductance).
So my conclusion would be that the TPSM84203 has a much better EMI behavior than the LMZM23601.
However, when i use the WEBENCH tool :
- If i don’t check the button « add en input EMI filter » with the selection « CISPR 22 class B » : the two modules LMZM23601 and TPSM84203 are proposed.
- But if i check button « add en input EMI filter » with the selection « CISPR 22 class B » : the LMZM23601v3 is proposed but not the TPSM84203.
I don’t understand why the TPSM84203 is not proposed in the second case as it seems to have better EMI performance (see above what i said about the datasheets). Is there something i didn’t understand ? Which modules is better to use for low EMI performances ?
Second small question unrelated with the previous one : the LMZM23601v3 is almost not available in the 4 majors electronic suppliers i know. I would have to wait for May 2022 before having those modules. I would like to know if it is temporary and due to the current worldwide shortage of electronics components or if it is a problem i can have often with this component.
Thank you in advance for your answer
Best regards