Hi Team,
There is a good new that we DIN TI LP8863ADCPRQ1!
Regarding the GD pin of LP8863, a resistor and a capacitor are connected to the ground. Can the RB7 resistor be replaced with 15 ohm?
CB24 is changed to 470pf , what effect will this have on the line?
Vmax:26.36V-LED OPEN
Vmin:5.11V-LED min
UVP:25V-OCP
4V x 6LED =24V