Other Parts Discussed in Thread: UCC28065
Hi,
I have question of UCC28064A. Please advise me.
What is VPHB_LR?
Is VPHB_LR a threshold voltage for the Phase-B turn-off in the case of 90 to 132 VRMS (US mains)?
What is VPHB_HR?
Is VPHB_LR a threshold voltage for the Phase-B turn-off in the case of 180 to 265 VRMS(European mains).?
What is VPHB?
What is relationship with VPHB_HR, VPHB and VPHB_LR?
Previous, I read the following Q and A, but, I can't understand the VPHB_LR and VPHB_HR.
If possible, please advice me including concrete examples.
Q
RU=133kohm, RD=47kohm, IPHB_range=3uA. The result is VPHB_LR=1.57V, VPHB_HR=1.67V. What is the relationship with VPHB_HR, VPHB and VPHB_LR?
A
Eq 10 gives you a threshold voltage for the Phase-B turn-off based on what power level you want with respect to max power. VPHB, which from an earlier response is 4.825V x 0.250 + 0.125 = 1.331V for Phase-B turn-off at Pout = 25%.
Once VPHB is calculated, it must be assigned to either VPHB_LR or VPHB_HR, and the other will be subject to the 3uA delta shift (up or down).
VPHB is each of them depending on which input voltage range you are targeting.
Best regards,
M.Takahara.