This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62912: Line Regulation Info

Part Number: TPS62912


Hello

I will use the TPS62912 to generate a 3.3V supply from 5-12VDC input voltage. First the input voltage will be 5VDC then it will change to 12V. I was looking for the line regulation specification in the datasheet to see how much the output voltage will change when the input voltage jumps from 5VDC to 12VDC. I cannot find any information about this in the datasheet.

Why this and how can I get the output stability instead?

Best regards
Robin