I have a problem with the bq40z60.
If I put the load( e.g. 500mA) to the vsys point on the refference schematic, the charging current will be 500mA ( charging current preset==1000mA).
If the load current increasing (e.g. 1500mA), the Current will be -500mA. Which means it drains the battery.
How can I set, if the adapter is on it, never drain the battery.
Thanks in advance,
Peter