HI all,
I've been handed some prototype boards to debug that use the LM22679-ADJ part to generate a 5V, 4A max output from a 9V to 19V input. This is the first time we are using this circuit. The output is stable for a given load but the output voltage decreases as the load increases [5V out at 100mA load, 4.3V at 4A load, the output oscillates with a 6A load]. I admit I'm not very experienced with this kind of thing. As the designer left the company and I don't have any of his design notes, I ran the design parameters through WEBENCH and the resulting component values match what was used.
Looking at the layout, the current loop could have been smaller so I did try adding a second output capacitor with the ground connection closer to the diode but this didn't help. The feedback voltage is clean and I am at a loss to understand why the circuit is not regulating.
Schematic:
Any guidance is appreciated. Thanks so much.