HI I'm design a AC to DC power
Q1. Imput AC 85~265 Vac out put DC 300V/3A
Q2. Imput AC 85~265 Vac out put DC 400V/0.5A
i see UCC28070 have EVM , but it only 300W
If i want change output power up to Q1 Q2 ,can you suggest T1 T2 L1 L2 D1 D2 Q1 Q2 Part number ?