Hi Team,
In the datasheet, Ivcc is spec'd at 65mA minimum. What is the worst case value for the current limit though? What is the maximum for that spec?
Thank you,
Jared
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
In the datasheet, Ivcc is spec'd at 65mA minimum. What is the worst case value for the current limit though? What is the maximum for that spec?
Thank you,
Jared
Hi Jared,
VCC regulator is an LDO and the only spec that matters is the guaranteed available VCC current, which is the min limit of Ivcc. It is because VCC regulator supplies the driver and its current capability can impact the driver performance. The design should be done such that it draws less than the Ivcc min limit. Therefore, the max limit does not mean much in a design, and we did not intentionally look for the max limit in the characterization.
Hope this explains.
Best Regards,
Youhao
Hi Youhao,
Thanks for the insight. The concern is not so much the driver performance, but there are scenarios where the VCC voltage is supplied from BIAS and it would be good to know the maximum potential current that can be drawn from the BIAS pin. Is that something you can provide?
Thanks,
Jared
Sounds good Youhao! If you do find any data on it, please let me know. Thanks!