Other Parts Discussed in Thread: BQ40Z50
I am struggling to find information on how the "Max Avg Dsg Current" battery lifetime value (section 14.8.2.3 in the BQ40Z50-R1 technical reference manual) is calculated.
Appendix B of the technical reference manual "Sample Filter Settings" mentions a flash setting "Calibration:Filter:Average V/I/P" which is used to configure the filter's time constants, with four example settings and their corresponding time constants. However, this flash setting is not listed in the "Calibration Data Flash" (section 11.2.1), or the "Data Flash Summary" (section 14.16), and as such no default value or address is given.
What is the sample rate of the current sensing?
How is the averaging of current samples performed?
If it is filtered, what is the time constant of this filter (or what does it default to if it can be configured)?
If it is a running average, across how many samples is the average taken?