Hi
The customer design with BQ24735. When only the adapter (DC 19V6A) is connected, the ACDET measures 2.8V and the system can be powered on.
When the lithium battery(3 series cells) is connected, the first 6s is pre-charge, and the charging current is set to 256mA. At this time, the charging circuit is normal.
When entering the normal charging and the charging current is 3A, ACFET and RBFET will turn on and off.
Please refer to the attached ACDET waveform, and the schematic.
Please give some suggestions.
Thanks
Star