Hi,
I am using BQ25790EVM to charge a 4S1P battery pack from a 12V input supply. Please find attached the setup picture. The evaluation board isn't charging the battery but the following conditions are valid:
1. The EN_CHG bit is set to 1 and CE pin is LOW.
2. No thermistor fault on TS pin.
3. No safety timer fault.
The battery voltage is @ 15.62V and I have attached register data for your reference. If you can point me in the right direction, that would be great.
* Created: Wed Sep 15 15:37:51 PDT 2021 * * Format: Register Name tab Character,\t Register Address tab Character,\t Hexadecimal register value. * Device: BQ25790_92 * BQZ Container: Charger_2_00-BQ25790_92.bqz * REG00 26 REG01 0690 REG03 0064 REG05 24 REG06 012C REG08 C3 REG09 05 REG0A E3 REG0B 00DC REG0D 4B REG0E 3D REG0F A2 REG10 10 REG11 40 REG12 00 REG13 01 REG14 16 REG15 AA REG16 C0 REG17 7A REG18 54 REG19 012C REG1B 0F REG1C 0A REG1D 01 REG1E 00 REG1F 00 REG20 00 REG21 00 REG22 00 REG23 00 REG24 00 REG25 00 REG26 00 REG27 00 REG28 00 REG29 00 REG2A 00 REG2B 00 REG2C 00 REG2D 00 REG2E 30 REG2F 00 REG30 00 REG31 0000 REG33 0000 REG35 0000 REG37 0000 REG37 0000 REG3B 0000 REG3D 0000 REG3F 0000 REG41 0000 REG43 0000 REG45 0000 REG47 00 REG48 01