Part Number: UCC28063
Other Parts Discussed in Thread: UCC28061
Dear Expert
Ctm change UCC28063 to UCC28061 ,and system fails to start .The Pin5 COMP is low lever ,other pin voltage are normal.
Below is schemetic ,pls check!24v8a.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, in order to help you, I need more information. The schematic you provided is using the UCC28061 controller.
1. Did the customer have a working solution with the UCC28061 and then change out the controller for a UCC28063?
2. If the answer to 1. is YES, what other circuit changes did the customer make to accommodate the differences between the -061 and 063 controllers? Please provide a schematic.
3. If the answer to 1. is NO, can you please explain the situation more clearly and with more details.
Thank you,
Ray
Hi Gabriel,
The UCC28063 is NOT a simple drop-in replacement for the UCC28061. The customer should consult the two datasheets to understand what is different between the two controllers and change their application accordingly.
Although many of the improvements made to the -063 will not require changes to the application circuit, some likely will. I've highlighted those features below:
COMP:
>COMP drive capability is lower, so attached circuitry must not overload it

> Need to make sure Flyback PFC mods do not interfere with COMP being able to reach <20mV
VINAC:
VSENSE: