Hi,
I am working with a TPS259824OEVM eval board. It is powered by a DC power supply (12 V) and outputs to an electronic load. I have confirmed that it has the default factory jumper configuration.
The eFuse cuts power at 3.2 A load. With the default jumper configuration, it should allow 5 A. But I can move the jumper to any setting on J10 and I get the same result.
This is an issue, because I have an eFuse implementation on a pcb that I designed that does not pass current under any circumstances. My plan was to verify operation on the EVM and then use the same values in my design.
Do you have any ideas about why the EVM is not performing as expected? Thank you!
-Kirk