We run these devices to convert out 48V bus to power some 5V devices. The component design and layout is basically the same as the example in the datasheet.
The bus power supply has a very high output capacitance due to needing to drive many other things.
In our application we do not require hot-plugging anywhere on this and have reasonable power on transients at all times.
However sometimes it can be that a loose cable or a maintenance worker will cause a very fast transient, or a hot-plugging of either the 48V line or the Gnd line.
Historically we have had a couple of rare reports of a boards get destroyed from "hot plug", but I am skeptical if this is really the case.
Can this buck be hot plugged at 48V?
Shouldn't there be something in the absolute max ratings that specifically states what the limits are on rise time transients or inrush currents?
Is there are low cost and readily available (ie: the chip crisis) part that I can add to my design in order to better protect it?
Perhaps a simple choke of some sort... is there a design document on how to add this? I would like to maintain the 600mA rating that this buck is rated for.
While I have plenty of voltage-drop headroom, I feel like an NTC would just create unnecessary heat and also its not so reliable for the issues like people messing with cables because the device stays hot for a period after power off and doesn't really protect well in this time. At least that's what I have read.
In some of my other designs i use the TPS2663x to achieve this (with different bucks and higher current requirements) however i feel that this component is over-kill for this application in terms of cost, added competent, footprint size and current market availability.