Hi expert,
I made a buck converter PCB using LM5101B. External High / Low signal is generated from MSP430.
The generated PWM signal has no problem at scope with proper dead time. And input & output waveform of low side is well synchronized.
But only high side waveform makes a big difference between input and output. The schematic is so simple as below,
The Vcc is 10V and FET gate is connected via 4,7ohm R.
What kind of condition can cause the kind of waveform mismatch at high side input and output ?
Thanks & regards,
YS Kim