Hello Team,
Thermal specs for TLV757P are described in datasheet section 6.4
RθJB Junction-to-board thermal resistance = 64.4 °C/W for SOT23-5 package
RθJB Junction-to-board thermal resistance = 64.3 °C/W for WSON package
...=> RθJB for SOT23-5 and WSON have same value (within 0.1);
...=> indicates that both packages are equal at conducting heat into PCB;
...=> indicates that junction temp shoud be same for both packages.
RθJA Junction-to-ambient thermal resistance = 231.1 °C/W for SOT23-5 package;
RθJA Junction-to-ambient thermal resistance = 100.2 °C/W for WSON package;
...=> RθJA for SOT23-5 is approx 2.31 x WSON;
...=> indicates that junction temp for SOT23-5 will be hotter than WSON for same power dissipation;
Can you explain why the RθJB ratio is the same for both packages but the RθJA ratio is 2.31?
Regards,
Renan