Hi Sir.
I am AMARA BASSAM from Renault Group company.
We need to design a board to convert 12V to 5V 3A
I share with you the schématic of this block
After test of this shcématic we find that the output voltage is all time in 10V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir.
I am AMARA BASSAM from Renault Group company.
We need to design a board to convert 12V to 5V 3A
I share with you the schématic of this block
After test of this shcématic we find that the output voltage is all time in 10V
HI
can I know which input you add in your circuit and when output all time in 10V, what is your feedback resistor value and what is the FB voltage?
Thanks
Hi Mister daniel.
Firt i think you for your quiqly answer.
the input is 12V.
the target is to convert input power 12V to 5V 3A.
The resistance in the pin 5 of LM2673 is 4.99 Ohm.
in the Feedback pin we have to resistor R1 and R2 1K Ohm.
I share the schématic of this small board
Thank you.
.
HI
if you use adj version of LM2673, with 1K ohm up and down feedback resistor, you should get 2.4V output voltage because internal Vref of adj version is 1.2V . Can you check the FB voltage, and make sure it is output adjustable version instead of fixed output version.
I think PIN 5 resistor is 4.99kohm instead of 4.99ohm, right?
Hi mister Daniel
i replace the R2 value by 3.3K ohm in pin 5 it is 4.99 Kohm
and i find this value of volatage pins
Pin 1 : 10.5V
Pin 2 : 12V
Pin 3 : 11.6V
Pin 4 : 0V
Pin 5 : 1.19V
Pin 6 : 0.00036V
Pin 7 : 4.36V
Thank you.
HI
Do you have output voltage? it looks you have voltage at PIN1 but no voltage at PIN 6, is there any connection or soldering issue?
Cause if PIN1 is 10.5V, Vo should have voltage around 10.5V, but FB(PIN 6) will sense the voltage by dvivide resistors ,it should have the votlage, based on your divide resistor,it should have around 1.75V
Thanks