Hello, I want to make board for wireless project. Project will be powered from 2x series LR20 battery (3.2V max). Power consumtion on 3.3V is less than 0.1mA while sleeping (most of time). non sleep current max 100mA. Power consumption is 0.1mA while sleeping (most of time) and max 1A while working. Need tips how to make it as effective as possible (optimalisation of current consumption at 0.1mA level. There are my questions:
1) Is TPS61030 good idea for this project for 3.3V and 5V? Will be it effective at 0.1mA? (can't find informations in datasheet)
2) Is it good idea to do 5V with TPS61030 and then 3.3V from 5V with TPS62740? (3.3V made from voltage after converter, it will affect quality of 3.3V?)
3) Maybe TPS61030 for 5V and TLV61220 for 3.3V is better idea?
4) What values and types of passive components would you recommend to make 3.3V and 5V LC filter after converters to get good quality voltages for MCUs?
5) Any suggestions what other converters I should choose?
Looking forward to hearing from you!