This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2660: Customer using TPS26602 with non-standard connection from OVP to RTN

Part Number: TPS2660

Hi Experts

My customer is using TPS26602 but has connected OVP to RTN using a 3k ohm and/or 3 ohm instead of the recommended 0 ohm value.

I have asked them to confirm whether there are any other nets/resistors also connected to OVP and will provide that information as soon as I have it.

What will be the effect on device behavior if the OVP to RTN connection is higher than the intended 0 ohms?

Best regards,

Jim B