Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM, EV2400
Hi,
Previously i used the 3000mAh batteries cell with BQ40z80.
Now i am using the new 4000mAh batteries. However i still see Qmax 3150mAh on the bsq.
Also, the SOC is 7% with 25.2V battery. I think the SOC is incorrect (SOC should be higher for this 25.2V). Please refer to attached figure.
What do i need to do after programming the correct chemistry ID to the BQ40Z80 (Battery ID 5441)? Do i need to do calibration or learning cycle for new battery on BQ40Z80 so that to get correct SOC?
Thanks!