Other Parts Discussed in Thread: TPS53515
Hi,
Can we take TPS53515 as a replacement of TPS548A20 at 7A design?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mingkun,
Our US team will check and reply you soon.
Yes, they are pin-compatible devices. TPS53515 is a 12A converter. The TPS548A20 is a 15A converter with different FETs (9.9mΩ & 4.3mΩ vs. 13.8mΩ & 5.9mΩ).