Hello,
I have a question about the footprint for the TPS22946 load switch presented in the datasheet versus the one available in the Ultra Librarian site.
In the datasheet of the TPS22946, the recommended pad diameter is 0.225 mm, but in the Ultra Librarian footprint it is 0.305mm.
What pad size should be used and would you need to add solder mask expansion?
Or is the footprint in Ultra Librarian ok to be used as-is?
Thanks!