Folks:
There are several typos in the Device Data Sheet (SLUSC76C –JULY 2015–REVISED MAY 2018):
Also, the PMID signal (the direct, unswitched output of the Boost converter) could use a more-detailed
description. Is it allowed to draw current from that pin? The documentation only shows it ever connected
to a filter capacitor but as long as one isn't looking for the reverse-blocking help of the RBFET, it looks like
it should be valid to draw +5 V from PMID:
Atlant