Other Parts Discussed in Thread: DAC81416,
Greetings community,
I'm currently having a ripple issue using the LMZ3004 as a inverter to generate -12V from a 12V input. It is current limited at 700 mA by a current limiter IC. The -12V output is used to feed the VSS supply pins of DAC81416.
I'm driving the 16 output channels with a 2k load on each (5 mA at +/-10V range). I'm using a parallel load with a dip switch to toggle some of the channels between 5mA and 25mA, as the datasheet mentions it can drive up to 25mA on each output. The problem I'm observing goes as follow: With the 10V output range with the DAC, I'm observing that the limiter is effectively working after enabling up to 7 switches for changing the loads.
I'm using 4 DACs in my actual design, the mentioned with up to 7 switches toggles to drive a load of 25 mA and the rest is driven at 5mA on each outputs. So that makes a total of :
-9 channels at 5mA == 285 mA
- seven switched channels at 25mA == 175 mA ,
- the supply current drawn by each of the 4 DACs Vdd , 25 mA each according to the datasheet (100mA total)
- the supply current drawn by the Vss supplies of the 4 DACs, 60 mA and since the the efficiency of the LMZ34002 is about 85% : roughly 110 mA
- 285 + 175 + 100 + 110 == 670 mA
Considering the precision of the loads, this amount of current seems like the threshold for my current limiter.
But then, when I switch the range to -10V, the issue occurs :
The overcurrent fault occurs at a much lower current threshold, as I'm only able to toggle 3 switches, which makes roughly a difference of 80 mA.
Also, the ripple observed at the LMZ input is about twice as bad , about 200 mV pp.
I'm using 10uF ceramic low ESR decoupling capacitor as per recommend by the datasheet, tried a 4.7uF also, the ripple remains the same.
I'm wondering if somebody might have a clue about what I'm observing, I can provide more details if necessary :)
Kind Regards