Other Parts Discussed in Thread: LM74700-Q1
When these parts are configured in a OR-ing configuration, will the loads still be protected from reverse polarity?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When these parts are configured in a OR-ing configuration, will the loads still be protected from reverse polarity?
Hi Jeffrey,
LM74610-Q1 does not have reverse current blocking functionality (which is key for OR-ing functionality) when the input voltage is positive. Hence LM74610-Q1 is not suitable for OR-ing configuration. LM74610-Q1 is suitable only for input reverse polarity protection.
You can consider using LM74700-Q1. This device supports both input reverse polarity protection and reverse current blocking (thus, OR-ing) functionalities.