Dear Team,
Do we have file can share TPS23881 power consumption for 90W POE output for internal thermal simulation?
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
I don't believe we have thermal simulation for this device. However, since the IC is external FET, the power dissipation would be limited to the controller operating power at VPWR and VDD. We've done this calculation before and it is ~0.5W which corresponds to a ~35C temp rise at the junction. So at room temperature, the IC will be ~60C which is well below the max Tj of the part. Please let us know if this helps. Thanks!