Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ12003: LMZ1200x enable pin internal pull-up value

Part Number: LMZ12003

Hello!

 I would like to know the resistance value of internal pull-up between EN and VIN pin.

Thanks,

Marina.

  • Hi ,

    Our expert will check this soon.

    BRs,

    Young

  • Hi Marina,

     Could you tell me why you need this internal resistance value? Usually we will not disclose the internal information to customer.

    Thanks,

    Nancy

  • We need it because in one of our designs we connect the EN pin of LMZ  to a +5V signal (with an external pull-down of 10K). We supply the LMZ with 12V.

    If the +5V signal is in high impedance, which would be the expected value in EN pin? I guess that current would fllow through internal pull-up from 12V to EN, and maybe we would see voltage on EN pin (which is connected to +5V in our design). That could be a problem for us. 

  • Hi Marina,

    The internal resistor from Vin to EN should be pretty high from datasheet 8.2.2.1 section as below.

    We could not find the exactly value since the previous engineer is not at TI. Actually you don't need to know that value.

    When you add 5V external voltage to EN pin. The voltage on EN pin would be 5V. The current flow through the internal resistor from Vin to EN does not affect your application.

    Hope this helps,

    Thanks,

    Nancy

  • Hello Nancy,

    thanks for your answer but it didn't resolve my issue. We need to know the value because we are doing a failure analysis of our desing. To create the +5V we have a converter with external inductance. We need to analyze what happens when this inductor is in open-state.What voltage can we expect in +5V/EN? Our external pull-down resistor is 10K, maybe you don't know the exact value of the internal pull-up resistor, but would it be around 10K, 100K, 500K?

    I add a diagram to clarify it.

  • Hi Marina,

    Understand, from the equation 1 in the datasheet, I derived the resistor value with more than 1Mohm. you can use 1Mohm.

    If the inductor is open, The EN pin will be 5V definitely and no need to do math calculation.

    Thanks,

    Nancy

  • OK! Thank you.

    Only one question, if  'L' on scheme is in open state, the voltage on EN pin would be set by the resistive divider formed by Rpull-up internal (aroung 1Meg) and Rpull-down external (10K); so the EN pin voltage would be around 0V. Is is correct?

  • Hi Marina,

    If the 5V comes from the left side of inductor, that is correct. 

    Thanks,

    Nancy