Hello,
Class 8 PD specifies a 63.4 ohm resistor. Can a 64.9 ohm resistor be used instead? Or will that cause problems?
Thanks,
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Class 8 PD specifies a 63.4 ohm resistor. Can a 64.9 ohm resistor be used instead? Or will that cause problems?
Thanks,
Michael
Hey Michael,
Yes a 64.9ohm resistor should be okay. The IC will place 2.5V across the resistor when there is a class finger. The current needs to be between 36mA and 44mA for a Class 4 signature. Note for IEEE802.3.bt standard, class 8 is technically a class 4 signature and a class 3 signature.
For V/R =I >>> 2.5V / 64.9ohm = 38.5mA, so I think we should be good.
Just note that the class current is 38.5mA, so typically this resistor is 0805 or larger size. Can't do a 0402
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments