Is it safe to install a 10 ohm current limiting resistor between the voltage source and the part's Vin? The goal is to limit the inrush current to a few hundred milliamps during power up.
The input source voltage is 3.3V and the output capacitance is 1400 uF.
My concern is that the inrush current spike will cause the input voltage to droop below 2V and cause the part to dither on/off as the 3.3V supply ramps up.
My DC load current is less than 20 mA so I am not so concerned about the ~0.2V drop across the resistor during steady state operation.
Thanks.