Hi,
I have a problem with the dropout voltage of VIN.
The maximum value of VDO (VIN) in ”6.5 Electrical Characteristics” is 165mV,
but in Figure 6, the maximum value I can get under the same situation ( VBIAS-VOUT = 3.25V,Iout = 1.5A ) is only ~83mV.
I want to know how the maximum value of 165mV is obtained, why these two values have almost doubled, and how to confirm this maximum value in my design
My spec, VIN=2.5V, VBIAS= 5V, Vout= 1.8V, IOUTmax= 500mA
Best regards,
Xiwu