Part Number: BQ24120
Other Parts Discussed in Thread: BQ24104, BQ24109, BQ24103
Can you confirm that the only difference between BQ24120 and BQ24104 are the following?
Pin 2 - STAT1 (behavior)
- BQ24120 – either ON or OFF
- BQ24104 – either ON or OFF or alternating ON/OFF (0.5Hz interval)
Pin 13 – CELLS (NC in BQ24120)
- BQ24120 – NC
- BQ24104 – CELLS: ground or float for 4.2V, single-cell operation. Pull-up resistor to VCC for 8.4V, two-cell operation.