This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610EVM: BQ24610EVM can not charge full

Part Number: BQ24610EVM

Hi

The customer use BQ24610EVM to charge the 5S1P lithium battery.  The lead from the battery pack to the BAT is about 8 cm, and TS connect a 10K resistor to the ground.

At the beginning of charging, everything is normal. At the end, the STAT1 blink, and STAT2 can not turn on.

The VBAT voltage is about 20V and does not reach 21V. The current value jumps from 0 to less than the termination current. 

The DC power supply is 24V.

Why can not terminate the charge?

Waiting for your reply.

Thanks

Star